Wince 13 not booting in iMX6 sabre sdb

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Wince 13 not booting in iMX6 sabre sdb

1,760 Views
srikanthmediset
Contributor I

Hi,

   I have downloaded wince 13 binaries from witekio website and I tried to flash the binaries using cfimage in to sabre sdb. But I am not getting any boot menu in the console.I had set the boot switch to boot from sd card correctly.I am not getting what I was missing.

Regards

srikanth.

Labels (3)
0 Kudos
Reply
1 Reply

1,635 Views
igorpadykov
NXP Employee
NXP Employee

Hi Srikanth

one can check if correct image was used as "sabre sdb" is generic

name for several boards with different processors: i.MX6Q, DL, SX.

For procedure issues may be sense to contact witekio directly as nxp

does not support wince on i.MX6 platform.

Witekio | Witekio contact 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply