Dear All,
my board design is based on SabreSD . There is a strange issue that board will auto turn on automatically even whole system is turned off (battery always mount).
I have double check the snvs_lp part which is alarm source to generate wake up to linux/android kernel.
My kernel is 3.0.35, android release is android_jb_4.2.2_1.1.0. Does anyone ever encounter issue like that?
Just to further add some point as I realize that if the suspend period is short, issue may not appear; I have tested 5 mins suspend seems to cause the issue to appear consistently - point 2. "alrm_time" may be zero value initially, suspend the board for at least 5 mins & then resume the board, the "alrm_time" will become non-zero value. So to list the steps again:
Hi Peter,
Thanks for your advice. Issue can be reproduced on both our android_jb4.3_1.1.0-ga & android_kk4.4.2_1.0.0 images running on Freescale Rev C4 SDP board. Customer reported this issue on their Rev B3 SDP running android_jb4.3_1.1.0-ga. Steps to reproduce:
There is no need to set the Android system alarm for the issue to occur, instead dependency is on the "alrm_time" read out by the command root@sabresd_6dq:/ # cat /proc/driver/rtc . "alrm_time" is initially zero when the image is freshly loaded, but it will automatically be filled up with some value after some suspend & resume.
Best regards
Sock Keng