Will any GPIO interrupt wake-up the iMX6DL from deep sleep?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Will any GPIO interrupt wake-up the iMX6DL from deep sleep?

477件の閲覧回数
ismaeltorres
Contributor I

I see in the documentation that while the iMX6DL is in deep sleep, only keypad, GPIO, and SNVS will wake it up. But the question is if any of the GPIO interrupts is wake up capable or only some of them, like those listed as GPIO1 0-7 / INT0-7.

Thanks.

Ismael.

ラベル(1)
0 件の賞賛
返信
1 返信

382件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ismael

yes any GPIO interrupt is capable to wake up

from low power modes.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信