Will L4.14.98-2.0.0_ga BSP run on original MCIMX8M-EVK?

cancel
Showing results for 
Search instead for 
Did you mean: 

Will L4.14.98-2.0.0_ga BSP run on original MCIMX8M-EVK?

511 Views
mindchasers
Contributor III

Hello,

We have been using the NXP L4.14.98-2.0.0_ga BSP with the MCIMX8M-EVKB.  We're in need of more EVKB systems but are only finding the original EVK systems in distribution.

Will the L4.14.98-2.0.0_ga BSP & Linux kernel run on the original EVK board?   We don't want to support two different kernel images & BSPs for our development.

Thank you,

Bob

0 Kudos
1 Reply

462 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Bob,

Yes, the image generated for the L4.14.98-2.0.0_ga BSP will run on the original MCIMX8M-EVK as well.

I hope this helps!

Regards,

0 Kudos