WiFi Scan not working in Android Auto

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

WiFi Scan not working in Android Auto

983 次查看
mayanksirotiya
Contributor I

Hello All,

I am working on iMX8QXP-CPU MEK. And I have flashed following pre-built Android Auto image downloaded from NXP portal.

android_p9.0.0_1.0.2-auto-beta_image_8qmek

I have ported my WLAN driver for this board, and able to install the module.

Using CLI, I am able to bring up my interface and connect to an AP. ping is also working fine.

However, I have couple of questions :-

1. I tried setting following

setprop wifi.interface <interface_name> && setprop wifi.direct.interface <interface_name>

still not able to scan available networks using GUI.

Is there is anything else I need to do for making this work?

2. I cannot find dhcp running in this image. Also do not know how to start this.

As a result, I have to assign ip manually.

Is there any command to start dhcp? To help resolving ip address automatically?

Many Thanks,

Mayank

0 项奖励
回复
1 回复

887 次查看
CarlosCasillas
NXP Employee
NXP Employee

Hi Mayank,

The i.MX8QX series is still on preproduction, so, no additional information/support could be provided yet. In case of having doubts, please refer with your Sales/FAE.


Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

-------------------------------------------------------------------------------

0 项奖励
回复