I want to add a WiFi/BT module on imx8qxp-mek, i find the Murata Type 1CX M.2 EVB seems like available.
But from the introduction manual i notice that to active the module evk,it should be load the specified dtb in uboot,like:
setenv fdt_file fsl-imx8mq-ea-com-kit_v2-pcie.dtb or fsl-imx8mq-evk-pcie1-m2.dtb
In addition,the document said that using “meta-murata-wireless” to hooked into the yocto build and create the sdacard image.
But in Industry-leading Wi-Fi +Bluetooth/BLE Connectivity Solutions for all i.MX Products.pdf shows:
cause i have two question:
1,i want to confirm that whether the murata 1CX m.2 evk available for imx8qxp-mek?
2,As mentioned above,how could i make any further development on board what if i want modified the configuration of hardware?
thank you!
Hi Peterson
for m2 modules one can look at
wireless.murata.com/eng/products/rf-modules-1/wi-fi-bluetooth-for-freescale-i-mx.html
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi @igorpadykov,
We have Murata-Module LBEE5HY1MW-230 available and connected with IMX8MQuad. We are using the L5.4.47_2.0.0 release.
from reference site : https://wireless.murata.com/products/rf-modules-1/wi-fi-bluetooth-for-nxp-i-mx.html#Linux
"Linux 4.1.15, 4.9.11, 4.9.88, and 4.9.123 are supported by Murata-enabled fmac Backports"
Does NXP has tested with L5.4.47 ?
Thanks
>Does NXP has tested with L5.4.47 ?
for tested chips one can look at Table 8. Supported features, p.16
Best regards
igor