Hi all,
I wondering about 'Debug LED and SDXC Power Control Inverter' of I.MX6DL(Automotive) SABRE Bd Circuit.
And I wondering about what purpose of 'SDa_RST_B' and 'SDa_PWROFF' , 'USER_LED', 'P3V3_SDa_SWITCHED'
And, Is 'Debug LED and SDXC Power Control Inverter' circuit must to use?
Best Regards,
Inho Jeon.
已解决! 转到解答。
Hello,
If Your design is not intended to use both voltages 3.3V and 1.8 V for SD
interface and SD supply will not be switched on / off - the mentioned solution
with switched supply may be ommited. In such case You may use P3V3_DELAYED
instead of P3V3_SDa_SWITCHED.
Regards,
Yuri.
Hi, Yuri!
I have a question about "SDa (SD3) power source for MX6 I/O. Required for SDXC USH-1 I/O logic level change " of i.MX6DL(Automotive) that refer to SABRE BD Schematics( 6 of 22 pages).
I want to NVCC_SD3 is P1V8GEN4 for SDXC(high speed SD IO level 1.8V).
So, I'll designed just R613 & R640 for NVCC_SD3 level control by add & del R640,R631 without U508(ADG849) and SDa_VSELECT(SD3_VSEL_GPIO_18), Is it right way?
Plaese, Infome me that questions, ASPA.
Best Regards,
Inho Jeon.
Hi, Yuri!
Thank you for your reply.
You mean just need to parts of R640 & R631 for driving SD or SDXC memory cards, no need to parts of 'U508' ,'R633', 'C625',R638 and net of 'SDa_VSELECT(SD3_VSEL_GPIO_18)', is that right?
Best regards,
Inho Jeon
Hello,
1.
Dedug LED is separate scheme, that – generally has no any concern to SDXC support.
2.
For the SDXC card support it is required to apply 1.8V supply voltage.
GPIO_18 (ALT2: VSELECT of usdhc3) is used to control the NVCC_SD3 for 3.3V and 1.8V voltage select.
SD3_RST(inverted to SDa_PWROFF) is used to control / switch the SD Card Power (P3V3_SDa_SWITCHED).
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Yuri,
Thank you for your reply.
You mean if not use SDXC it is not necessary, is that right?
And, if not use SDXC, how to design about "SDa_RST_B(SD3_RST)" , "P3V3_SDa_SWITCHED" ?
Best Regards,
Inho Jeon
Hello,
If Your design is not intended to use both voltages 3.3V and 1.8 V for SD
interface and SD supply will not be switched on / off - the mentioned solution
with switched supply may be ommited. In such case You may use P3V3_DELAYED
instead of P3V3_SDa_SWITCHED.
Regards,
Yuri.