Why target fails to power off on IMX6 sabre auto

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Why target fails to power off on IMX6 sabre auto

1,438 Views
huyadi
Contributor I

1: Boot IMX6 board (only sabre auto)

2:Use "poweroff" or "shutdown -h 0" commands

3: target is still alive

I tested with freescale's sdk based 3.10 branch, the target fails to power off too.

git://git.freescale.com/imx/linux-2.6-imx.git

git branch * imx_3.10.17_1.0.0_ga "

pm_power_off function works well on sabreSD target via operate regiester on rtc-svns.c, it seems rtc-svns can not power off sabre auto,   do you know why it is and how to power it off?

thanks a lot

0 Kudos
Reply
3 Replies

982 Views
igorpadykov
NXP Employee
NXP Employee

Hi hu

sabre auto has different circuitry related to pmic_on_req,

like J5 (Automatic Power On) on SCH-27142.pdf, so one can check it.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

982 Views
huyadi
Contributor I

Hi

I can't figure out what your  said,  I mean  kernel seems to be properly shut downed, but pm_power_off() doesn't cut off the electric power,

system remains in powered state

do you know which FSL's kernel version can resolve the issue?

Yadi

0 Kudos
Reply

982 Views
huyadi
Contributor I

Hi

thanks your reply,  but I attempted to lift J5 jumper  according to Quick Start Guide.

   J5:

     1–2 CAN control of system power

     2–3 Processor control of system power (default)

the target stiil fails to power off with both setting, do you know why?

thanks advance.

0 Kudos
Reply