Why only 4.1 for imx6ulevk?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Why only 4.1 for imx6ulevk?

1,587 次查看
oskar_nilsson
Contributor I

I'm working on porting a imx6ul based board from 4.1 to 4.9. I have been successful at getting it to run on 4.9, but I'm a bit concerned that the "official" default is only 4.1, a few other variants of imx6ul boards are on 4.14.

What is "holding" the imx6ulevk back from using 4.9?

From http://freescale.github.io/doc/release-notes/2.5/

imx6ul-pico-hobbitlinux-fslc4.14+git
imx6ul-pico-pilinux-fslc4.14+git
imx6ulevklinux-fslc-imx4.1-2.0.x+git
标签 (1)
0 项奖励
回复
1 回复

1,387 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Oskar

official nxp software is described on

i.MX Software|NXP 

linux-imx - i.MX Linux kernel 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复