Why is meta-qt5 in imx-5.4-24-2.1.0 using master branch instead of zeus

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Why is meta-qt5 in imx-5.4-24-2.1.0 using master branch instead of zeus

跳至解决方案
2,772 次查看
MikeEngel
Contributor IV

Hi,

we have started to port our Yocto BSP to the latest release imx-5.4.24-2.1.0 and have seen that the meta-qt5 layer points in the manifest to the master branch and not like the rest of the repos to the zeus branch.

Is this a error or why has that change been done?

Best regards,

--

Mike Engel

标记 (3)
1 解答
2,687 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello Mike, 

The BSP confirmed that this configuration is as intended. The reason why the Qt5 layer is taken from the master branch is to allow the upgrade to get Qt 5.15 with vulkan support. This layer was tested and should work correctly even trough it's not taken from the Zeus branch.

I hope this information helps. Thank you for pointing this out. I'm sure other Community users will ask the same question.

Regards,

在原帖中查看解决方案

4 回复数
2,687 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello Mike Engel,

Thank you for pointing this out. Let me investigate whether this was deliberate or not, albeit I would expect that it should use also a Zeus based commit. I’ll let you know as soon as I have more information.


Regards,

0 项奖励
回复
2,687 次查看
MikeEngel
Contributor IV

Hi Gusarambula,

thanks for the quick response. Yes it is a little bit strange that all repos are pointing in the manifest to zeus except meta-qt5.

I will wait for further information from you. Thanks

Best regards,

--

Mike

0 项奖励
回复
2,688 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello Mike, 

The BSP confirmed that this configuration is as intended. The reason why the Qt5 layer is taken from the master branch is to allow the upgrade to get Qt 5.15 with vulkan support. This layer was tested and should work correctly even trough it's not taken from the Zeus branch.

I hope this information helps. Thank you for pointing this out. I'm sure other Community users will ask the same question.

Regards,

2,687 次查看
MikeEngel
Contributor IV

Hello Gusarambula,

Thanks for the information and clarifying this.

Best regards,

--

Mike

0 项奖励
回复