Why is meta-qt5 in imx-5.4-24-2.1.0 using master branch instead of zeus

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Why is meta-qt5 in imx-5.4-24-2.1.0 using master branch instead of zeus

ソリューションへジャンプ
2,764件の閲覧回数
MikeEngel
Contributor IV

Hi,

we have started to port our Yocto BSP to the latest release imx-5.4.24-2.1.0 and have seen that the meta-qt5 layer points in the manifest to the master branch and not like the rest of the repos to the zeus branch.

Is this a error or why has that change been done?

Best regards,

--

Mike Engel

タグ(3)
1 解決策
2,679件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Mike, 

The BSP confirmed that this configuration is as intended. The reason why the Qt5 layer is taken from the master branch is to allow the upgrade to get Qt 5.15 with vulkan support. This layer was tested and should work correctly even trough it's not taken from the Zeus branch.

I hope this information helps. Thank you for pointing this out. I'm sure other Community users will ask the same question.

Regards,

元の投稿で解決策を見る

4 返答(返信)
2,679件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Mike Engel,

Thank you for pointing this out. Let me investigate whether this was deliberate or not, albeit I would expect that it should use also a Zeus based commit. I’ll let you know as soon as I have more information.


Regards,

0 件の賞賛
返信
2,679件の閲覧回数
MikeEngel
Contributor IV

Hi Gusarambula,

thanks for the quick response. Yes it is a little bit strange that all repos are pointing in the manifest to zeus except meta-qt5.

I will wait for further information from you. Thanks

Best regards,

--

Mike

0 件の賞賛
返信
2,680件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Mike, 

The BSP confirmed that this configuration is as intended. The reason why the Qt5 layer is taken from the master branch is to allow the upgrade to get Qt 5.15 with vulkan support. This layer was tested and should work correctly even trough it's not taken from the Zeus branch.

I hope this information helps. Thank you for pointing this out. I'm sure other Community users will ask the same question.

Regards,

2,679件の閲覧回数
MikeEngel
Contributor IV

Hello Gusarambula,

Thanks for the information and clarifying this.

Best regards,

--

Mike

0 件の賞賛
返信