Why i.MX6ULL do not log in

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Why i.MX6ULL do not log in

1,313 Views
FrontMan
Contributor I

Please I am having trouble getting started with my NXP i.MX6ULL board, the user guide is not helping me as it stated that that the board will prompt "Industrio log-in" on the computer screen but I saw nothing of such. Please can anyone help me out with a step by step solution......Thanks.

here is my email also: isong.nathan90@gmail.com 

Enabling IW416 Bluetooth on iMX8MM(UART2) + Linux BS

MYS-6ULX Single Board Computer for Industry 4.0 and IoT Applications @

0 Kudos
Reply
2 Replies

1,304 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Could you tell us which version of BSP are you using on your board?

1,296 Views
FrontMan
Contributor I

Well I do not know hot to determine that but here is more info about the board.....

OVERVIEW.

IDO-EVB6Y09 is a development board for NXP i.MX6ULL . It is developed based on the IDO-SOM6Y08 core board. It is equipped with NXP IMX6ULLIEC processor and the maximum frequency can reach 800MHz. Support WIFI Bluetooth module and 4G full Netcom module wireless communication mode, provide dual Ethernet interface, CAN, RS-485, RS-232, USB OTG, TF card, SIM card, LVDS, RGB, TP and audio and other functional interfaces . It can be used as an evaluation board or widely used in various industrial Internet of Things gateways and industrial control equipment.

0 Kudos
Reply