Please I am having trouble getting started with my NXP i.MX6ULL board, the user guide is not helping me as it stated that that the board will prompt "Industrio log-in" on the computer screen but I saw nothing of such. Please can anyone help me out with a step by step solution......Thanks.
here is my email also: isong.nathan90@gmail.com
Enabling IW416 Bluetooth on iMX8MM(UART2) + Linux BS
MYS-6ULX Single Board Computer for Industry 4.0 and IoT Applications @
Could you tell us which version of BSP are you using on your board?
Well I do not know hot to determine that but here is more info about the board.....
OVERVIEW.
IDO-EVB6Y09 is a development board for NXP i.MX6ULL . It is developed based on the IDO-SOM6Y08 core board. It is equipped with NXP IMX6ULLIEC processor and the maximum frequency can reach 800MHz. Support WIFI Bluetooth module and 4G full Netcom module wireless communication mode, provide dual Ethernet interface, CAN, RS-485, RS-232, USB OTG, TF card, SIM card, LVDS, RGB, TP and audio and other functional interfaces . It can be used as an evaluation board or widely used in various industrial Internet of Things gateways and industrial control equipment.