Hi!
When comparing imx-gpu-viv-6.2.4.p1.0-aarch64 with imx-gpu-viv-6.2.4.p0.2-aarch64 there is one strange difference. The file gbm_viv.so is depending on libwayland-server in version 6.2.4.p1.0 but not in 6.2.4.p0.2. I can't see any reason why one would need to build libwayland-server.so just to use the GPU on a framebuffer system.
To test this:
$ readelf -a imx-gpu-viv-6.2.4.p0.2-aarch64/gpu-core/usr/lib/gbm_viv.so | grep NEEDED
0x0000000000000001 (NEEDED) Shared library: [libdrm.so.2]
0x0000000000000001 (NEEDED) Shared library: [libGAL.so]
0x0000000000000001 (NEEDED) Shared library: [libc.so.6]
$ readelf -a imx-gpu-viv-6.2.4.p1.0-aarch64/gpu-core/usr/lib/gbm_viv.so | grep NEEDED
0x0000000000000001 (NEEDED) Shared library: [libdrm.so.2]
0x0000000000000001 (NEEDED) Shared library: [libGAL.so]
0x0000000000000001 (NEEDED) Shared library: [libwayland-server.so.0]
0x0000000000000001 (NEEDED) Shared library: [libc.so.6]
It would be great to get a explanation why this change was added or if this is a configuration error.
Best regards,
Erik
Hi Erik,
It makes sense for gbm_viv.so to have dependency on libwayland_server.so since it hooks up gbm and wayland.
It has been recently added.
It is not available yet in early release version p0. It is normal you didn't see it.
Okay, it might make sense. I'm not that familiar with gbm.
But then I have a new question. Why do NXP provide a "-fb" version of libEGL, libGLESv2 etc.
-rwxr-xr-x 1 erik erik 1183656 mar 12 16:25 libEGL-fb.so
lrwxrwxrwx 1 erik erik 12 apr 20 14:02 libEGL.so -> libEGL-fb.so
lrwxrwxrwx 1 erik erik 12 apr 20 14:02 libEGL.so.1 -> libEGL-fb.so
lrwxrwxrwx 1 erik erik 12 apr 20 14:02 libEGL.so.1.0 -> libEGL-fb.so
-rwxr-xr-x 1 erik erik 1353256 mar 12 16:28 libEGL-wl.so
-rwxr-xr-x 1 erik erik 1138032 mar 12 16:24 libEGL-x11.so
If I can't run the framebuffer only version what's the reason for having "-fb" version and which should I use?
Best regards
Looks like it's related to this post: