Why does add IC add IC NC7WV16 between IMX8 mini Enthernet ENET_RX[0:3] and AR8031

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Why does add IC add IC NC7WV16 between IMX8 mini Enthernet ENET_RX[0:3] and AR8031

1,420 Views
wangchqin
Contributor I

Why does add IC add IC NC7WV16 between IMX8 mini Enthernet ENET_RX[0:3] and AR8031  , if I want  change AR8031 to  RTL 8211E  ,  if the  IC NC7WV16 is need ?

0 Kudos
Reply
3 Replies

1,415 Views
joanxie
NXP TechSupport
NXP TechSupport

refer to the schematic,

Drivers are included in the receive path due to long signal paths
and board-to-board connector. Adopters should place the PHY and
processor on the same board, and eliminate the drivers. Refer to
Atheros documentation for additional guidance

 

0 Kudos
Reply

1,412 Views
wangchqin
Contributor I

if I use another PHY  as RTL8211F (with normal  driver) ,  and let  the MAC and PHY  in one board without B to B connector ,  can I  omit   IC NC7WV16 ?

0 Kudos
Reply

1,405 Views
joanxie
NXP TechSupport
NXP TechSupport

yes you can omit it

 

0 Kudos
Reply