Why do I get the print 'imx2-wdt 20bc000.wdog: Device shutdown: Expect reboot!'

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Why do I get the print 'imx2-wdt 20bc000.wdog: Device shutdown: Expect reboot!'

3,232 Views
ramanareddy
Contributor I

Hi,

I see the following print whenever I reboot the board.

imx2-wdt 20bc000.wdog: Device shutdown: Expect reboot!

Why do I get this print ? Is this a bug in my image?

Tags (2)
0 Kudos
1 Reply

2,018 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ramana

please refer to Chapter 48 Watchdog (WDOG) Driver

attached Linux Manual and check that driver was properly included in image.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos