Why boot up time is different by boot I/F

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Why boot up time is different by boot I/F

3,519 Views
ko-hey
Senior Contributor II

Hi all

I'm using i.MX6 and i.MX USB Loader.
We hope to shorten the writing time of FW during board production.

The operation method is going to proceed below.

1. When manufacturing the board, mounting a blank FROM (eMMC)
2. Boot the board in Serial Downloader mode and transfer boot file from UART 1
3. Write FW to eMMC

Compared the processing speed of 3 and Internal Boot (eMMC), it takes quite a while in Serial Donwloader mode.

Boot files use the same thing and the performance seems to be different depending on Boot I / F.

Why does the boot time is different ?


If the serial downloader mode can boot up as same speed as Internal Boot, we can reduce the production time.

Please advise me.

・Linux(L4.1.15_2.1.0_ga)
http://git.freescale.com/git/cgit.cgi/imx/linux-imx.git/

・i.MX USB Loader
https://github.com/boundarydevices/imx_usb_loader.git


Ko-hey

0 Kudos
Reply
13 Replies

3,199 Views
fabio_estevam
NXP Employee
NXP Employee

Hi Ko-hey,

Which i.MX6 are you using?

Maybe this patch can help you:

[U-Boot] [PATCH 2/3] imx: Enable ACTLR.SMP bit for Cortex-A7 platforms 

Regards,

Fabio Estevam

3,199 Views
ko-hey
Senior Contributor II

Hi Fabio Estevam

They use i.MX6UL (MCIMX6G2CVM05AA).

Thank you we'll try it.

Ko-hey

0 Kudos
Reply

3,199 Views
fabio_estevam
NXP Employee
NXP Employee

Hi Ko-Hey,

MX6UL has a CortexA7 core, so the patch I mentioned should fix the slow transfer in serial download mode.

Regards,

Fabio Estevam

0 Kudos
Reply

3,199 Views
ko-hey
Senior Contributor II

Hi FabioEstevam

We're trying it and using the following as u-boot.
A) http://git.freescale.com/git/cgit.cgi/imx/uboot-imx.git

I think that the patches taught are targeted for the following items.
B) http://git.denx.de/u-boot.git

Q1. The implementation is quite different in the above A), B).

which one should be used in the first place ?


Q2. If you should use A), how should we patch it ?

Ko-hey

0 Kudos
Reply

3,199 Views
fabio_estevam
NXP Employee
NXP Employee

Hi Ko-Hey,

This fix has already been applied in the NXP U-Boot imx_v2017.03_4.9.11_1.0.0_ga version:

http://git.freescale.com/git/cgit.cgi/imx/uboot-imx.git/commit/?h=imx_v2017.03_4.9.11_1.0.0_ga&id=79... 

Regards,

Fabio Estevam

0 Kudos
Reply

3,199 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

  Two reasons for the different times.

 

1.

  Difference between eMMC read and write operations.

 

2.

  i.MX boot ROM provides SD port initializations for internal

boot mode (from SD), but for the serial downloader mode

SD port is configured by default.

 


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,199 Views
ko-hey
Senior Contributor II

Hi YuriMuhin_ng

Thank you for reply.

Do you have any idea for booting with SD port initializations in the serial downloader mode ?

Ko-hey

0 Kudos
Reply

3,199 Views
Yuri
NXP Employee
NXP Employee

Hello,

 Boot ROM in the serial downloader mode does not initializes SD. 

This is prerogative of application / system, that is loaded to i.MX under

the serial downloader mode.  

Regards,

Yuri.

0 Kudos
Reply

3,199 Views
ko-hey
Senior Contributor II

Hi YuriMuhin_ng

So I can't reduce the boot time when I use the serial downloader mode. 

Am I correct ?

Ko-hey

0 Kudos
Reply

3,199 Views
Yuri
NXP Employee
NXP Employee

Yes. Boot ROM code cannot be modified. 

0 Kudos
Reply

3,199 Views
ko-hey
Senior Contributor II

Hi Yuri Muhin

Okay, I understand.

Do you have any idea to speed up boot time in serial downloader mode ?

Ko-hey

0 Kudos
Reply

3,199 Views
Yuri
NXP Employee
NXP Employee

Hello,

  what do You mean?

Please describe the scenario of using the serial downloader mode. 

Regards,

Yuri.

0 Kudos
Reply

3,199 Views
ko-hey
Senior Contributor II

Hi Yuri Muhin

Sorry to bother you again.

As I say, we hope to shorten the writing time of FW during board production.

In board production, we plan to use i.MX USB Loader and download via UART.

So if you have any idea to reduce the writing time, pleas share us.

Ko-hey

0 Kudos
Reply