Why are pad controls for LCD pins 0x10 (invalid speed field)?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Why are pad controls for LCD pins 0x10 (invalid speed field)?

ソリューションへジャンプ
2,057件の閲覧回数
ThomasG1z
Contributor III

I see in e.g. the devicetree files for e.g. the SabreSD or Nitrogen6x that the pad control for all the relevant pins for the LCD parallel interface are set to 0x10. Why is that? It means that the SPEED field is set to 00 which is reserved according to the reference manual. Is there a particular reason, something I've overlooked or just an error..?

pinctrl_ipu1: ipu1grp {
fsl,pins = <
MX6QDL_PAD_DI0_DISP_CLK__IPU1_DI0_DISP_CLK 0x10

...

0 件の賞賛
返信
1 解決策
1,864件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

yes, pad controls of the Dual/Quad are similar to Solo/Duallite

and next Solo/Duallite RM will be updated with this info.

~igor

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,864件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi ThomasG1z

setting Speed 00 LOW — Low frequency (50 MHz)

according to i.MX6DQ RM

MX6DQRM  rev.2  7_2014     p.2290.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,864件の閲覧回数
ThomasG1z
Contributor III

I see now that the documentation has been changed from the 2013 to 2014 version currently listed on your site. However for the i.MX6S/DL the reference manual on your web pages are still from 2013 and the speed field is documented like this:

pastedImage_0.png

But I assume the pad controls of the Dual/Quad are similar to Solo/Duallite so this field is not really reserved??

0 件の賞賛
返信
1,865件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

yes, pad controls of the Dual/Quad are similar to Solo/Duallite

and next Solo/Duallite RM will be updated with this info.

~igor

0 件の賞賛
返信