Why are all Qt windows full screen in i.mx6q Qt 5.xxx ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Why are all Qt windows full screen in i.mx6q Qt 5.xxx ?

759 Views
bluedrum
Contributor I

I am using Qt5.8 to port a project in imx6q.

Qt 5.8 from NXP yocto .

I found that all windows (such as dialogs, main window) are forced to display full screen.

No matter how you adjust setWindowFlag(), it is always full screen.

The original layout was completely destroyed,

Hard to see the eglfs mode only full screen?

Labels (4)
0 Kudos
Reply
1 Reply

629 Views
igorpadykov
NXP Employee
NXP Employee

Hi Andrew

one can try with nxp bsps and follow sect.5.6.7 Qt 5 attached Yocto Guide.

linux-imx - i.MX Linux kernel 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply