Why VGEN5 is changed from 2.8V to 3.0V on i.MX6Q SABRE?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Why VGEN5 is changed from 2.8V to 3.0V on i.MX6Q SABRE?

跳至解决方案
699 次查看
satoshishimoda
Senior Contributor I

Hi community,

Our customer have a question about i.MX6DQ SABRE and Linux BSP.

Please see the schematics of i.MX6Q SABRE platform, VGEN5_2V8 is used for VDDHIGH_IN power supply.

And VGEN5 is changed the output voltage from 2.8V to 3.0V by u-boot.

Our customer want to know why it is changed to 3.0V.

We know the min voltage to i.MX6DQ VDDHIGH_IN has been changed to 2.7V, so we think 2.8V supply from VGEN5 is no problem.

Although, the voltage changing has been remained in u-boot of latest BSP.

Would you let me know the reason?

Best Regards,

Satoshi Shimoda

标签 (3)
0 项奖励
1 解答
510 次查看
art
NXP Employee
NXP Employee

The VGEN5 voltage is increased to 3.0V to make it able to supply the VDD_SNVS_IN rail in full run mode as well.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
4 回复数
511 次查看
art
NXP Employee
NXP Employee

The VGEN5 voltage is increased to 3.0V to make it able to supply the VDD_SNVS_IN rail in full run mode as well.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
510 次查看
satoshishimoda
Senior Contributor I

Dear Artur,

Would you reply my above question?

Our customer want to know the meaning of "full run mode".

Best Regards,

Satoshi Shimoda

0 项奖励
510 次查看
art
NXP Employee
NXP Employee

As "full run mode" I mean the mode when all supply voltages, including VDD_HIGH_IN, are applied to the processor.

Artur

0 项奖励
510 次查看
satoshishimoda
Senior Contributor I

Dear Artur,

Thank you for your reply.

> The VGEN5 voltage is increased to 3.0V to make it able to supply the VDD_SNVS_IN rail in full run mode as well.

Did you mean " To supply when VDD_SNVS_IN draw 1mA since VSNVS can supply up to 400uA"?

Best Regards,

Satoshi Shimoda

0 项奖励