Hi community,
Our customer have a question about i.MX6DQ SABRE and Linux BSP.
Please see the schematics of i.MX6Q SABRE platform, VGEN5_2V8 is used for VDDHIGH_IN power supply.
And VGEN5 is changed the output voltage from 2.8V to 3.0V by u-boot.
Our customer want to know why it is changed to 3.0V.
We know the min voltage to i.MX6DQ VDDHIGH_IN has been changed to 2.7V, so we think 2.8V supply from VGEN5 is no problem.
Although, the voltage changing has been remained in u-boot of latest BSP.
Would you let me know the reason?
Best Regards,
Satoshi Shimoda
已解决! 转到解答。
The VGEN5 voltage is increased to 3.0V to make it able to supply the VDD_SNVS_IN rail in full run mode as well.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
The VGEN5 voltage is increased to 3.0V to make it able to supply the VDD_SNVS_IN rail in full run mode as well.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Dear Artur,
Thank you for your reply.
> The VGEN5 voltage is increased to 3.0V to make it able to supply the VDD_SNVS_IN rail in full run mode as well.
Did you mean " To supply when VDD_SNVS_IN draw 1mA since VSNVS can supply up to 400uA"?
Best Regards,
Satoshi Shimoda