Why RPMSG size is changed on A9 core in latest BSP imx-5.4.24-2.1.0.xml from 0x8000 to 0x10000 ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Why RPMSG size is changed on A9 core in latest BSP imx-5.4.24-2.1.0.xml from 0x8000 to 0x10000 ?

Jump to solution
1,002 Views
rakesh_patel
Senior Contributor I

Old BSP with kernel 4.1.15

============

&rpmsg{
compatible = "fsl,imx6sx-rpmsg";
reg = <0x9FFF0000 0x8000>;
status = "okay";
};

 

New BSP with kernel 5.4

============

&rpmsg{
vdev-nums = <1>;
compatible = "fsl,imx6sx-rpmsg";
reg = <0x9FFF0000 0x10000>;
status = "okay";
};

 

Query:

================

1) Why RPMSG size change on A9 core only? Does it not required on M4 side as well?

2) What is the calculation to change size from 0x8000 to 0x10000?

Labels (1)
0 Kudos
Reply
1 Solution
975 Views
igorpadykov
NXP Employee
NXP Employee

Hi rakesh_patel

 

usually for bsp changes no additional documents provided except on official nxp linux link:

https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...

 

Also nxp official L4.1.15 bsp (from codeaurora.org/external/imx/linux-imx repository) has not such entry :

https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm/boot/dts/imx6sx-sdb-m4.dts?h=imx_...

 

Old BSP with kernel 4.1.15

============

&rpmsg{
compatible = "fsl,imx6sx-rpmsg";
reg = <0x9FFF0000 0x8000>;
status = "okay";
};

 

Best regards
igor

View solution in original post

0 Kudos
Reply
3 Replies
997 Views
igorpadykov
NXP Employee
NXP Employee
0 Kudos
Reply
981 Views
rakesh_patel
Senior Contributor I

@igorpadykov :

Thanks for sharing the open-forum links.

But, I want some useful information from NXP's documents for changing size in A9 core in new BSP and no change in M4 side.

Please do needful for the same.

0 Kudos
Reply
976 Views
igorpadykov
NXP Employee
NXP Employee

Hi rakesh_patel

 

usually for bsp changes no additional documents provided except on official nxp linux link:

https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...

 

Also nxp official L4.1.15 bsp (from codeaurora.org/external/imx/linux-imx repository) has not such entry :

https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm/boot/dts/imx6sx-sdb-m4.dts?h=imx_...

 

Old BSP with kernel 4.1.15

============

&rpmsg{
compatible = "fsl,imx6sx-rpmsg";
reg = <0x9FFF0000 0x8000>;
status = "okay";
};

 

Best regards
igor

0 Kudos
Reply