Dear Analog experts,
I'm not familiar with OP Amp.
When I measured MMPF0100/F0 PMIC output timing, most of SWx turned on just in time(Sq# x 2ms).
Why only VREF DDR output so delayed to start turn-on?
It seems to kept on low around 400us.
Can anybody help me?
Thanks
Solved! Go to Solution.
Hi,
This delay that you are seen is probably caused by a big capacitance in the layout VREFDDR line, I believe that this delay can probably be adjusted by modifying the output capacitor value on VREFDDR pin. Try using a lower value capacitor.
Have a great day,
Jose Reyes
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
This delay that you are seen is probably caused by a big capacitance in the layout VREFDDR line, I believe that this delay can probably be adjusted by modifying the output capacitor value on VREFDDR pin. Try using a lower value capacitor.
Have a great day,
Jose Reyes
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
BTW
I reviewed VINREFDDR then found SW3AB supplied 1.5V to VINREFDDR.
Suppose if VINREFDDR>0.8V then mos FET goes ON, it takes 512us where slewrate set 25mV/16us.
BR