Who can tell me, how to use imx6 csi2 MIPI_CSI_DATA_IDS_x and ipux_csix_di.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Who can tell me, how to use imx6 csi2 MIPI_CSI_DATA_IDS_x and ipux_csix_di.

955 Views
guanliangding
Contributor III

Who can tell me, how to use imx6 csi2 MIPI_CSI_DATA_IDS_x and ipux_csix_di.

0 Kudos
Reply
2 Replies

693 Views
igorpadykov
NXP Employee
NXP Employee

Hi guanliang

for virtual channel explanation with example one can look at

Some Experience When Enable MIPI Camera

DATA_IDS_1 and DATA_IDS_2 are for matching error reporting

(optional) with some descriptions in register MIPI_CSI_ERR1,

sect.40.6.9 Error state register 1 (MIPI_CSI_ERR1) RM.

For general steps one can look at attached document from sdk

sect.18.5.1.2 High-speed serial interface-MIPI, sect.22.7 Initializing the driver.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

693 Views
guanliangding
Contributor III

Hi, igor:

     Thank.

     I have read it. But now, i can't make sure the data flow is ok. Now status is dphy is 0x300 and no error. I think the mipi-csi2 layer is ok.

B.R    

     John

0 Kudos
Reply