Who can give me some guide about how to compile and package a new package in ltib?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Who can give me some guide about how to compile and package a new package in ltib?

2,925件の閲覧回数
zhiyancao
Contributor II

In ltib, I can compile all package provided by ltib release L2.6.35_10.11.01_ER_source_bundle.tar.gz, it can generate a rootfs directory.

But, this time, Provided the rootfs is not exist. I create a new package, for example vmware-open-client, I got source tar, and create the spec, I run ./ltib -m prep -p vmware-open-client, it is ok.

next step, ./ltib -m scbuild -p vmware-open-client, it can not work:

czy@czy-virtual-machine:~/imx51/ltib$ ./ltib -m scbuild vmware-open-client

The options prep, scbuild, scinstall and scdeploy are only allowed when working

on a single package, not a list.  You need to supply the option -p|--pkg <pkg>

czy@czy-virtual-machine:~/imx51/ltib$ ./ltib -m scbuild -p vmware-open-client

Processing: vmware-open-client

================================

Build path taken because: directory build, build key set, no prebuilt rpm,

rpmbuild --dbpath /home/czy/imx51/ltib/rootfs//var/lib/rpm --target arm --define '_unpackaged_files_terminate_build 0' --define '_target_cpu arm' --define '__strip strip' --define '_topdir /home/czy/imx51/ltib/rpm' --define '_prefix /usr' --define '_tmppath /home/czy/imx51/ltib/tmp' --define '_rpmdir /home/czy/imx51/ltib/rpm/RPMS'  --define '_mandir /usr/share/man' --define '_sysconfdir /etc' --define '_localstatedir /var' -bc --short-circuit  /home/czy/imx51/ltib/dist/lfs-5.1/vmware-open-client/vmware-open-client.spec

Building target platforms: arm

Building for target arm

Executing(%build): /bin/sh -e /home/czy/imx51/ltib/tmp/rpm-tmp.60960

+ umask 022

+ cd /home/czy/imx51/ltib/rpm/BUILD

+ cd vmware-open-client-4.5.0

+ ./configure --prefix=/usr --host=arm-linux --build=i686-pc-linux-gnu

Configuring VMware-view-open-client 4.5.0-297975

checking build system type... i686-pc-linux-gnu

checking host system type... arm-unknown-linux-gnu

checking which interface to build... Gtk+

checking for arm-linux-pkg-config... no

checking for pkg-config... /opt/freescale/ltib/usr/bin/pkg-config

configure: WARNING: In the future, Autoconf will not detect cross-tools

whose name does not start with the host triplet.  If you think this

configuration is useful to you, please write to autoconf@gnu.org.

checking pkg-config is at least version 0.9.0... yes

checking for GLIB... configure: error: Package requirements (glib-2.0 >= 2.6.0 gmodule-2.0 >= 2.6.0) were not met:

No package 'glib-2.0' found

No package 'gmodule-2.0' found

Consider adjusting the PKG_CONFIG_PATH environment variable if you

installed software in a non-standard prefix.

Alternatively, you may set the environment variables GLIB_CFLAGS

and GLIB_LIBS to avoid the need to call pkg-config.

See the pkg-config man page for more details.

error: Bad exit status from /home/czy/imx51/ltib/tmp/rpm-tmp.60960 (%build)

RPM build errors:

    Bad exit status from /home/czy/imx51/ltib/tmp/rpm-tmp.60960 (%build)

Build time for vmware-open-client: 1 seconds

Failed building vmware-open-client

f_scbuild() returned an error, exiting

traceback:

main:560

Exiting on error or interrupt

I want to know the following 2 tips:

No package 'glib-2.0' found

No package 'gmodule-2.0' found

how to solve it, I need to build and install glib-2.0 and gmodule-2.0 using ltib, and when they are in rootfs/usr/lib or some other directory?

ラベル(2)
0 件の賞賛
返信
5 返答(返信)

2,522件の閲覧回数
zhiyancao
Contributor II

I first build glib2,then scbuild vmware-open-client, now lack gtk+-2.0.

0 件の賞賛
返信

2,522件の閲覧回数
BrilliantovKiri
Senior Contributor I

Hello, zhiayn!

Unfortunally LTIB not supported package depends, you should be build if manually before target package.

0 件の賞賛
返信

2,522件の閲覧回数
zhiyancao
Contributor II

Thanks, I now manually building the depend packages, but I don't know which package will block me.

gtk+-2.0 is ok ,next is libcurl.

0 件の賞賛
返信

2,522件の閲覧回数
LeonardoSandova
Specialist I

Hi,

Adding a new package can be a pain, because it involves installing its dependencies as you have found out. Perhaps you already know how to create a .spec file, but take a look at this link

http://ltib.org/documentation-LtibFaq#ref_89

Leo

0 件の賞賛
返信

2,522件の閲覧回数
zhiyancao
Contributor II

vmware-open-client configure file check some header file, such as wchar.h, unicode/uidna.h;

wchar.h check is ok,

but unicode/uidna.h is not;

tips:

checking wchar.h usability... yes

checking wchar.h presence... yes

checking for wchar.h... yes

checking for SYS_setuid32... yes

checking for the new format of iconv... yes

checking whether sys/ucontext.h defines REG_EAX... no

checking unicode/uidna.h usability... no

checking unicode/uidna.h presence... no

checking for unicode/uidna.h... no

configure: error: libicu is required, but not found.  Check config.log for details.

where to find the header file when configure is running?

/opt/freescale/usr/local/gcc-4.4.4-glibc-2.11.1-multilib-1.0/arm-fsl-linux-gnueabi/arm-fsl-linux-gnueabi/include/

is right?

But wchar.h is ok, I copy unicode directory to the above dir, but configure can not find it.

0 件の賞賛
返信