Whitch mean description of clock frequency.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Whitch mean description of clock frequency.

跳至解决方案
1,294 次查看
takashitakahash
Contributor III

Description of IMX6SDL RM of  61.8.4.2 DIV2, PSR and PM Bit Description.

Description of [ NOTE

You must ensure that the bit-clock frequency must be never

greater than 1/5 of the peripheral clock frequency. The

oversampling clock frequency can go up to peripheral clock

frequency.]

This description of "Peripheral clock"are the ssi_clk_root or ipg_clk_root ?

标签 (1)
0 项奖励
回复
1 解答
1,159 次查看
Yuri
NXP Employee
NXP Employee

  According to Table 61-3 (SSI Clocks) of the RM, ipg_clk_root is peripheral clock

SSI_clcoks.jpg


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,160 次查看
Yuri
NXP Employee
NXP Employee

  According to Table 61-3 (SSI Clocks) of the RM, ipg_clk_root is peripheral clock

SSI_clcoks.jpg


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复