Which pin should be used as SD1_CD in SD/MMC manufacture mode?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Which pin should be used as SD1_CD in SD/MMC manufacture mode?

Jump to solution
1,243 Views
x10
Contributor V

Hi, all

SD/MMC manufacture mode is required to be implemented in my customized board which is based on iMX6UL. With RM, the signal SD1_CD_B can come from pad CSI_DATA05 (ALT8) or GPIO1_IO03 (ALT4) or UART1_RTS_B (ALT2). Please let me know which pin should be used as SD1_CD_B so that BOOT ROM can recognize the SD card on uSDHC1 interface. Thanks!

BR

Cheng Shi

Emtronix

Labels (1)
0 Kudos
Reply
1 Solution
989 Views
Yuri
NXP Employee
NXP Employee

Hello,

UART1_RTS_B (in ALT2 mode) is used as SD1_CD.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
4 Replies
989 Views
meriajacob
Contributor I

Hi,

The SD card is not detected in our board after power up. In our schematics, we have assigned the SD_CD pin to No Connect. We use the micro controller MCIMX7D7DVM10SC

But when we go in detail through the user manual its written, for embedded memory it should be tied to ground if not used. Will this cause an issue?

Kindly share your thoughts in this regard!!!!

Thanks,
Regards,
Meria Jacob

0 Kudos
Reply
989 Views
Yuri
NXP Employee
NXP Employee

Hello,

  

  From the i.MX7 DataSheet(s) : “uSDHC1 and uSDHC2 are primarily
intended to serve as external slots or interfaces to on-board SDIO devices.
These ports are equipped with “Card detection” and “Write Protection” pads .. ”.

  So, when using uSDHC1 and uSDHC2 for external slots with “Card

detection” signal, this signal should be grounded, if not used.

  Note, it is needed to have “Card detection” signal for SD boot (for uSDHC1
and uSDHC2, intended for external slots).

Regards,

Yuri.

0 Kudos
Reply
990 Views
Yuri
NXP Employee
NXP Employee

Hello,

UART1_RTS_B (in ALT2 mode) is used as SD1_CD.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
989 Views
x10
Contributor V

Thanks Yuri for quick reply.

BR

Cheng Shi

0 Kudos
Reply