Which is the best PMIC for i.MX 6 processor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Which is the best PMIC for i.MX 6 processor

630 Views
aneeshts
Contributor I

Hi

We are going to use i.MX 6 processor for our new projects and we have selected a PMIC from freescale(PF0100) but the there is some limitation for PF0100 IC the maximum input voltage is upto 4.5V for this IC. There is one more Ic from Linear(LTC3676) that will support upto 5.5V. Then we have the following doubts

1. which is the best PMIC For i.MX 6 processor( PF0100 or LTC3676)?

2. Can LTC3676 supports all the power requirement of i.MX 6 ?

3. If LTC3676 can supports then why everybody prefer PF0100 as first choice?

Regards

Aneesh

0 Kudos
1 Reply

377 Views
SergioSolis
NXP Employee
NXP Employee

The PF0100 was created with the i.MX6 in mind, thus enhancing its efficiency.

We already have system reference designs with it for faster time to market and a much better low power efficiency.

Here you can find all the application notes available and a fact sheet:

MMPF0100: 14 Channel Configurable Power Management Integrated Circuit

0 Kudos