Which i.MX6UL power mode wakes-up by keypad interrupt?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Which i.MX6UL power mode wakes-up by keypad interrupt?

跳至解决方案
1,371 次查看
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX6UL low power mode.

Out partner consider using keypad to wake-up from low power mode.

However, I did not find the information whether i.MX6UL can wake-up from low power mode and which power mode can wakes-up by keypad interrupt.

Would you give me the information?

Best Regards,

Satoshi Shimoda

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
1,236 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

wake-up with keypad can be used in all low power modes

except SNVS mode: all SOC digital logic, analog module are shut off

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,237 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

wake-up with keypad can be used in all low power modes

except SNVS mode: all SOC digital logic, analog module are shut off

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复