Which gstreamer plugin for iMX(8) is better ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Which gstreamer plugin for iMX(8) is better ?

Jump to solution
2,005 Views
khang_letruong
Senior Contributor III

Dear All,

I'm a little confused of which gstreamer-imx plugin that is most suitable for iMX8MM/iMX8MP board that I have. Concretely :

From Freescale repository, there's recent v2 branch that supports iMX8M, iMX8MM platforms : https://github.com/Freescale/gstreamer-imx

From NXP's Code Aurora repositories :
https://source.codeaurora.org/external/imx/imx-gst1.0-plugin/
https://source.codeaurora.org/external/imx/gst1.0-plugins-fsl/

Both have "i.MX Gstreamer 1.0 Plugin" in description.  

I would like then which one is better to be used with the following documentation :
https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8-GStreamer-User-Guide/ta-p/1098942

Thanks in advance and best regards,
Khang
 

 

Tags (1)
0 Kudos
Reply
1 Solution
1,991 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello  Khang,

The Gstreamer in the official is gstreamer 1.0 and comes from:

https://source.codeaurora.org/external/imx/imx-gst1.0-plugin/

 

You can find the documentation in the release notes and linux reference manual on your yocto BSP documents, for usage you can use the community.

 

Regards

 

View solution in original post

1 Reply
1,992 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello  Khang,

The Gstreamer in the official is gstreamer 1.0 and comes from:

https://source.codeaurora.org/external/imx/imx-gst1.0-plugin/

 

You can find the documentation in the release notes and linux reference manual on your yocto BSP documents, for usage you can use the community.

 

Regards