Which functions will be closed in suspend mode?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Which functions will be closed in suspend mode?

911 Views
charleshuang
Senior Contributor II

We don't have PMIC

But we have a MCU which can make system to sleep mode

We want to know when system in standby mode by SW command (echo mem > /sys/power/state)

Which of the following features will the CPU shut down?

VPU

GPU

L2 Cache

USB

PCIE

SATA

HDMI

LVDS

Or where can we refer in the documents?

Labels (2)
0 Kudos
Reply
1 Reply

796 Views
igorpadykov
NXP Employee
NXP Employee

Hi charles

all functions are disabled except snvs and wake capabilities,

details can be found in sect.18.5.3.3 STOP mode i.MX6DQ Reference Manual

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf

Table 9. Stop Mode Current and Power Consumption i.MX6DQ Datasheet

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply