Hi Ramana,
Yocto supports following compression filesystem formats:
btrfs
jffs2
cramfs
Please note Yocto provides support of many filesystem formats as it is collaborative project targeted for many architectures. Filesystem formats are related directly to the kernel but not the the BSP, and NXP does not manipulate the kernel when developing the BSPs, so you may investigate if the filesystem you wish to use is compatible with the mainline kernel you want to use.
These filesystems may work for you, however, NXP is not able to confirm they will work without issues as we have not tested on our images.
Below you can see a full list of formats supported by Yocto.
IMAGE_TYPES = " \
jffs2 jffs2.sum \
cramfs \
ext2 ext2.gz ext2.bz2 ext2.lzma \
ext3 ext3.gz \
ext4 ext4.gz \
btrfs \
iso \
hddimg \
squashfs squashfs-xz squashfs-lzo \
ubi ubifs multiubi \
tar tar.gz tar.bz2 tar.xz tar.lz4 \
cpio cpio.gz cpio.xz cpio.lzma cpio.lz4 \
vmdk \
vdi \
qcow2 \
hdddirect \
elf \
wic wic.gz wic.bz2 wic.lzma \
"
I hope this helps.
Regards,
Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------