Which exception level U-boot executes in iMX8MQ board?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Which exception level U-boot executes in iMX8MQ board?

1,135 次查看
yali_zhang
Contributor II

I used the "go" command to start an bare metal application. This is the SPSR:

SPSR: 601af1f1

HCR_EL2: 2
SCTRL_EL2: 30c51835

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

1,085 次查看
b36401
NXP Employee
NXP Employee

U-boot itself is running in EL2 and it runs the target in EL2 as well.
EL3 normally is reserved for the ARM trusted firmware, ROM etc.

0 项奖励
回复