Which eMMC 5.0 supports iMX6 series

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Which eMMC 5.0 supports iMX6 series

1,840 Views
kaushalbisht200
Contributor I

Dear NXP Team,

In our custom board we need to select eMMC for booting the board.

As I have gone through all your reference documents which says iMX6 series supports

eMMC Versions ( 4.3/4.3/4.4/4.41 ). But the problem is all these eMMC's are obsolete.

Many customer asked queries regarding eMMC5.0 support for iMX6 series and in

some cases NXP team saying it supports  and some saying it doesn't support.

links which says its supports eMMC 5.0

    https://community.nxp.com/message/663133

    https://community.nxp.com/message/642069

links which says it doesn't supports eMMC 5.0

    https://community.nxp.com/message/482971

    https://community.nxp.com/message/404575

Which eMMC 5 or greater version work with iMX6 series processor?

Please confirm, there is no problem in using eMMC 5.0/5.1 (HS200 or HS400) on

iMX6D processor. So that we can proceed with our designs.

Labels (3)
0 Kudos
2 Replies

865 Views
iohertz
Contributor II

Hello,

I am also designing using MCIMX6Y1. I am planning to use EMMC 5.0 for our product. But looks like some people are facing some problem with EMMC 5.0. I want to know what is the status of user posted this question. Have you received any success?

0 Kudos

865 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

You can refer EMMC 5.0 and EMMC 5.1 work on i.MX6 in our community. Hope it can help you.
Have a great day,
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos