Which bit is sent out first in iMX6 SPI interface

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Which bit is sent out first in iMX6 SPI interface

Jump to solution
1,339 Views
yangao
Contributor III

Hi,

For iMX6 SPI interface, when sending out data, is MSB sent out first or LSB sent out first?

Regards,

Winston

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,333 Views
Yuri
NXP Employee
NXP Employee

@yangao 
Hello,

   The MSB is output (first) when the host processor loads the transmitted data.

Regards,
Yuri.

View solution in original post

1 Reply
1,334 Views
Yuri
NXP Employee
NXP Employee

@yangao 
Hello,

   The MSB is output (first) when the host processor loads the transmitted data.

Regards,
Yuri.