Which SECO firmware version to be used with 5.15.52-2.1.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Which SECO firmware version to be used with 5.15.52-2.1.0

ソリューションへジャンプ
747件の閲覧回数
philippe_schenk
Contributor IV

Hello

We're currently integrating the NXP Release LF5.15.52_2.1.0 for our products based on i.MX 8 (QM and QP) and i.MX 8QXP (and DX).

For that I integrated the per Release Notes recommended SCFW 1.14.0. In the release notes document of the SCFW it is written that the SECO is tested against the following versions:

5.8.7: i.MX8DXL-A1/i.MX8DXL-B0
3.8.5: i.MX8QM/i.MX8QXP
1.1.6: i.MX8DXL-A1-V2X/i.MX8DXL-B0-V2X

 

In the "i.MX Linux Release Notes" it is suggested to use `imx-seco-5.8.7.1.bin` for "i.MX 8QuadMax, 8QuadXPlus, and 8DXL reference boards".

Could you elaborate which version of SECO we should use for SoCs i.MX 8QuadMax, i.MX 8QuadPlus, i.MX 8QuadXPlus, i.MX 8DualX together with SCFW 1.14.0 on release LF5.15.52_2.1.0?

Thanks and Best Regards,
Philippe

ラベル(1)
0 件の賞賛
返信
1 解決策
725件の閲覧回数
philippe_schenk
Contributor IV

We figured it out in the meantime. The SHA256SUM of the SECO from 3.8.5/3.8.6 and 5.8.7.1 are the same for the SoCs mentioned in the original question.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
726件の閲覧回数
philippe_schenk
Contributor IV

We figured it out in the meantime. The SHA256SUM of the SECO from 3.8.5/3.8.6 and 5.8.7.1 are the same for the SoCs mentioned in the original question.

0 件の賞賛
返信