Which PMIC is better for i.MX6UL: PF3000 or PF3001?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Which PMIC is better for i.MX6UL: PF3000 or PF3001?

1,341 Views
maximpodberezni
Contributor III


Hi!

I'm making a design based on imx6 UltraLite processor and want to use a PMIC. I have a reference design based on PF3000 but have not a similar one based on PF3001. The PF3001 product page states "The PF3001 is ideally suited for i.MX6UL processors", but I can't find any reference schematics for this PMIC. I can see little differences between these ICs, but I know how difficult it can be to bring up custom boards and just don't want to have lots of hardware iterations and a headache in software side.

Please suggest the best PMIC for imx6UL processor without problems to bring up the board and accessible from distributors

Labels (2)
Tags (1)
0 Kudos
3 Replies

763 Views
igorpadykov
NXP Employee
NXP Employee

Hi Maxim

PF3001 is simplified version of PF3000 and one can use both options.

For schematic please create service request.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos

763 Views
maximpodberezni
Contributor III

Hi Igor!

My distributor created the service request for SPF-28865, but it was for PF3000, not PF3001. Please suggest a number for the service request

0 Kudos

763 Views
igorpadykov
NXP Employee
NXP Employee

Hi Maxim

SCH-29090

Best regards

igor

0 Kudos