Which PCB material is the best? in i.mx9352

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Which PCB material is the best? in i.mx9352

1,169 次查看
vivek5676
Contributor III

Hi,

Please advice Which PCB material is the best? in i.mx9352.

Regards,

Vivek Kumar

0 项奖励
回复
2 回复数

1,134 次查看
vivek5676
Contributor III

Thanks !

0 项奖励
回复

1,142 次查看
joanxie
NXP TechSupport
NXP TechSupport

refer to the user guide, PCB material: the material used on EVK is 185HR.

for other material select, pls refer to this

Material characteristics such as the Coefficient of Thermal Expansion (CTE) should be considered. The CTE describes how a material changes dimension with temperature. Ideally, a PCB material’s CTE should be closely matched to copper, which is about 17 ppm°C. CTE is a concern because as the PCB expands during heating, it can elongate plated via holes and cause fracturing.
If the CTE is closely matched to copper, expansion of the PCB material and copper will be more uniform and the plated via holes will be more robust during thermal cycling.

0 项奖励
回复