Which Linux-5.10 branch in the linux-imx repo is recommended to run on i.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Which Linux-5.10 branch in the linux-imx repo is recommended to run on i.MX6

1,040 Views
MikeQi
Contributor I

Hi,

We plan to port Linux-5.10 onto our hardware platform which is based on i.MX6.

There are only two Linux-5.10 branches in the https://source.codeaurora.org/external/imx/linux-imx repo, their names are git.kernel.org/linux-stable/linux-5.10.y and lf-5.10.y. 

Which branch is recommended to run on i.MX6?  Do I need to wait for a Linux-5.10 branch whose name looks like imx_5.10.xx_x.x.x? I find some Linux-5.4 branches named in that way, e.g. imx_5.4.70_2.3.0 in the repo.

Thanks in advance

Labels (2)
0 Kudos
Reply
0 Replies