Hi all,
Anybody can tell which is the best PMIC for imx257 processor?. Somebody suggested me MC34704 PMIC for imx257. But when i went through the datasheet i found its having 3 buck boost, 1 buck, 1 inverter and 2 boost converter. but imx257 requires only 1.45V, 1.5V, 1.8V and 3.3V. simple buck regulators and LDO's are enough for this purpose. So i don't think MC34704 is the Best PMIC for Imx257 which is having some unwanted buck boost, inverter and boost. So anybody can suggest a good PMIC for imx257 from freescale as well as from other vendors?
Regards,
Aneesh
Hi ANEESH
seems one can find other pmics, for example TPS65051
however note that linux controls pmic (refer to attached document Chapter 5,6,7)
so one will have to develop own driver for new pmic.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------