Hi all:
Now we use embeded sync(EAV/SAV) to do line and frame sync.
But we find that some times the data signal be disturbed, then the protection bits(bit0-3) of EAV/SAV are not correct. so we want to disabe the protection bits checking.
I have try to call _ipu_csi_ccir_err_detection_disable in ipu_csi_init_interface(the original code is enable protection bits check by call _ipu_csi_ccir_err_detection_enable),
But it looks like not work, because I also can not capture any TVin video data.
So my question are:
1. how to disable the detection of EAV/SAV protection bits?
2. and if the protection bits is a wrong value, then whether we can capture the TVin video data?
Thank you very much!
Hi Liu
suggest to reinitialize IPU anew with disabled protection.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi igorpadykov:
Thank you for your response!
I checked _ipu_csi_ccir_err_detection_enable and _ipu_csi_ccir_err_detection_disable.
I find that these functions is just called at ipu_csi_init_interface,
Whether I can just reinit csi at mxc_v4l_open and mxc_v4l2_s_param function? because just these two functions will call ipu_csi_init_interface.
Thank you!
Hi igorpadykov:
I add following code to re-init IPU in mxc_v4l_open and mxc_v4l2_s_param of mxc_v4l2_capture.c
But it also can not capture any data.
Do you have some other suggest?
Thank you very much!
static int mxc_v4l_open(struct file *file)
{
...
ipu_csi_set_window_size(cam->ipu, cam->crop_current.width,
cam->crop_current.height,
cam->csi);
ipu_csi_set_window_pos(cam->ipu, cam->crop_current.left,
cam->crop_current.top,
cam->csi);
ipu_csi_init_interface(cam->ipu, cam->crop_bounds.width,
cam->crop_bounds.height,
cam_fmt.fmt.pix.pixelformat,
csi_param);
+#if 1 //re-init for disable ccir error detect
+ipu_csi_set_window_size(cam->ipu, cam->crop_current.width,
+ cam->crop_current.height,
+ cam->csi);
+ipu_csi_set_window_pos(cam->ipu, cam->crop_current.left,
+ cam->crop_current.top,
+ cam->csi);
+ipu_csi_init_interface(cam->ipu, cam->crop_bounds.width,
+ cam->crop_bounds.height,
+ cam_fmt.fmt.pix.pixelformat,
+ csi_param);
+#endif
clk_prepare_enable(sensor->sensor_clk);
vidioc_int_s_power(cam->sensor, 1);
vidioc_int_init(cam->sensor);
vidioc_int_dev_init(cam->sensor);
From experts:
-----------------------------------------------------------------
1. Customer can set the bit CSIx_CCIR_ERR_DET_EN from register IPUx_CSIx_CCIR_CODE_1 to 0 in order to disable the error detection and correction.
To make a quick test, customer can use /unit_tests/memtool to set and verify this bit.
2. I have never seen this issue before and I don't know what's the consequence of wrong protection bits.
-----------------------------------------------------------------
Best regards
igor