Whether can we update IMX8QM but not need Set the boot pin to serial download mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Whether can we update IMX8QM but not need Set the boot pin to serial download mode

Jump to solution
977 Views
wang12zhe
Contributor III

From the IMX_YOCTO_PROJECT_USERS_GUIDE.pdf, find need Set the boot pin to serial download mode mode first.

But whether can we update IMX8QM but not need Set the boot pin to serial download mode? 

 

0 Kudos
Reply
1 Solution
941 Views
AldoG
NXP TechSupport
NXP TechSupport

Hi,

Yes your understanding is correct.

Best regards,
Aldo.

View solution in original post

0 Kudos
Reply
3 Replies
965 Views
AldoG
NXP TechSupport
NXP TechSupport

Hello,

It is recommended to set serial download mode when you're testing software, since the device will go to serial download directly so you may update software.

For production it is possible to set Boot mode fixed, be it by fuses or GPIO to the desired boot media (eMMC, SD, NAND, etc.), since boot media would be clean at first boot, the device will go to serial download so it is possible to flash the device.

Best regards,
Aldo.

0 Kudos
Reply
962 Views
wang12zhe
Contributor III

@AldoG 

Thanks very much

I had test it, but one question:

After clean the first boot by command and reboot the system by command reboot

then download image by uuu, it will not start download process

the process only start when Disconnect and reconnect power, am I right

 

0 Kudos
Reply
942 Views
AldoG
NXP TechSupport
NXP TechSupport

Hi,

Yes your understanding is correct.

Best regards,
Aldo.

0 Kudos
Reply