Where to submit patches for linux-2.6-imx

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Where to submit patches for linux-2.6-imx

2,320 次查看
sarahn
Contributor I

Hi,

There is a very serious bug in the i.mx6 v4l capture drivers that I have a patch for.  These drivers appear to be specific to the BSP and do not exist in mainline. The email address referenced in Submit i.MX53 & i.MX28 Linux kernel patches appears to no longer be valid.  Can someone please post an update?  Also, should patches to i.mx related files which exist in mainline be submitted to the same list or is there a better place to do it?

Thanks, Sarah

标签 (1)
0 项奖励
回复
5 回复数

1,934 次查看
LeonardoSandova
Specialist I

Is this patch already on community Yocto BSP? If not, you may send a patch to the list and wait for approval.  (I do not know the Freescale channels for receiving outside patches....)

0 项奖励
回复

1,934 次查看
sarahn
Contributor I

I think having the patch applied in git instead of in yocto is preferable because it's possible to mix and match between kernel versions and distributions. 

If there is no official list, maybe an employee could sign off on it?  I could email it to the freescale employees who previously worked on that driver.

0 项奖励
回复

1,934 次查看
SergioSolis
NXP Employee
NXP Employee

The git to upload patches would be: Freescale · GitHub

0 项奖励
回复

1,934 次查看
Ragan_Dunham
NXP Employee
NXP Employee

Sarah,

Please attach the patch here; we'll review and determine whether to apply internally.

Thanks,

Ragan

1,934 次查看
sarahn
Contributor I

Thanks Ragan, I've attached the patch as you requested.  It applies cleanly against imx_3.10.31_1.1.0_alpha and imx_3.10.17_1.0.0_ga.

0 项奖励
回复