Where to find small cheap TFT LCD for QSB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where to find small cheap TFT LCD for QSB

670 Views
danix
Contributor III

Hi all,

I want to use parallel RGB TFT LCD w/ touch (2.8" - 3.5") and a resolution of at least 320x480 with the QSB, but I don't seem to find a good deal with that.

I'd appreciate a lot if you give me a link etc. where I can buy such displays in small quantity for a fair price.

Tags (1)
0 Kudos
2 Replies

607 Views
danix
Contributor III

Hi Manu,

I have seen those, but that one is 4.3" with a resolution less than the minimum I need ;(

Thanks anyway.

0 Kudos

607 Views
ManuMartinez
Contributor I

http://search.digikey.com/es/en/products/NHD-4.3-480272MF-ATXI%23-T...

Is hard to find small screens with resolution higher than QVGA (well is easy to find them in mobile phones :P). I hope these one be useful.

Regards.

0 Kudos