Where to find CCM_CSCDR3 register in Linux L3.10.53

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where to find CCM_CSCDR3 register in Linux L3.10.53

976 Views
dipalidhumal
Contributor I

Hi,

We are using i.MX6DL- (MCIMX6U8DVM10AC).

We need to modify CCM_CSCDR3 register values.

Please let us know where to get this register in Linux L3.10.53 from freescale.

Please let me for more information.

Regards,

Dipali

Labels (2)
0 Kudos
Reply
4 Replies

847 Views
saurabh206
Senior Contributor III

Hi Dipali,

You can use memtool utility to modify register.

If you have yocto setup available than you can generate using bitbake imx-test.

Thanks

Saurabh

0 Kudos
Reply

847 Views
dipalidhumal
Contributor I

Hi,

We don't want to try this option with memtool utility.

We have to make it in Linux.

Please see below file and tell us the steps and procedures to be changed.

./arch/arm/mach-imx/clk-vf610.c:#define CCM_CSCDR3        (ccm_base + 0x1c)

./arch/arm/mach-imx/clk-vf610.c:    clk[VF610_CLK_QSPI0_EN] = imx_clk_gate("qspi0_en", "qspi0_sel", CCM_CSCDR3, 4);

./arch/arm/mach-imx/clk-vf610.c:    clk[VF610_CLK_QSPI0_X4_DIV] = imx_clk_divider("qspi0_x4", "qspi0_en", CCM_CSCDR3, 0, 2);

./arch/arm/mach-imx/clk-vf610.c:    clk[VF610_CLK_QSPI0_X2_DIV] = imx_clk_divider("qspi0_x2", "qspi0_x4", CCM_CSCDR3, 2, 1);

./arch/arm/mach-imx/clk-vf610.c:    clk[VF610_CLK_QSPI0_X1_DIV] = imx_clk_divider("qspi0_x1", "qspi0_x2", CCM_CSCDR3, 3, 1);

./arch/arm/mach-imx/clk-vf610.c:    clk[VF610_CLK_QSPI1_EN] = imx_clk_gate("qspi1_en", "qspi1_sel", CCM_CSCDR3, 12);

./arch/arm/mach-imx/clk-vf610.c:    clk[VF610_CLK_QSPI1_X4_DIV] = imx_clk_divider("qspi1_x4", "qspi1_en", CCM_CSCDR3, 8, 2);

./arch/arm/mach-imx/clk-vf610.c:    clk[VF610_CLK_QSPI1_X2_DIV] = imx_clk_divider("qspi1_x2", "qspi1_x4", CCM_CSCDR3, 10, 1);

./arch/arm/mach-imx/clk-vf610.c:    clk[VF610_CLK_QSPI1_X1_DIV] = imx_clk_divider("qspi1_x1", "qspi1_x2", CCM_CSCDR3, 11, 1);

./arch/arm/mach-imx/clk-vf610.c:    clk[VF610_CLK_DCU0_EN] = imx_clk_gate("dcu0_en", "dcu0_sel", CCM_CSCDR3, 19);

./arch/arm/mach-imx/clk-vf610.c:    clk[VF610_CLK_DCU0_DIV] = imx_clk_divider("dcu0_div", "dcu0_en", CCM_CSCDR3, 16, 3);

./arch/arm/mach-imx/clk-vf610.c:    clk[VF610_CLK_DCU1_EN] = imx_clk_gate("dcu1_en", "dcu1_sel", CCM_CSCDR3, 23);

./arch/arm/mach-imx/clk-vf610.c:    clk[VF610_CLK_DCU1_DIV] = imx_clk_divider("dcu1_div", "dcu1_en", CCM_CSCDR3, 20, 3);

./arch/arm/mach-imx/clk-vf610.c:    clk[VF610_CLK_NFC_PRE_DIV] = imx_clk_divider("nfc_pre_div", "nfc_en", CCM_CSCDR3, 13, 3);

Regards,

Dipali

0 Kudos
Reply

847 Views
art
NXP Employee
NXP Employee

The listing you've provided is for VF6 series Vybrid controllers platform. Try

to find the same for MX6DL platform. Also, check the corresponding device tree file:

arch/arm/boot/dts/imx6dl.dtsi


Have a great day,
Artur

0 Kudos
Reply

847 Views
dipalidhumal
Contributor I

Hi Artur,

Thanks.

We have gone through the dtsi file as you mentioned and could not find any reference to CCM_CSCDR3.

PFB listing for imx processor which is the only reference regarding this register we found in the kernel code.

./arch/arm/mach-imx/crm-regs-imx5.h:#define MXC_CCM_CSCDR3        (MX51_CCM_BASE + 0x3C)

./arch/arm/mach-imx/crm-regs-imx5.h:#define MXC_CCM_CSCDR3_HSI2C_CLK_PRED_OFFSET        (16)

./arch/arm/mach-imx/crm-regs-imx5.h:#define MXC_CCM_CSCDR3_HSI2C_CLK_PRED_MASK        (0x7 << 16)

./arch/arm/mach-imx/crm-regs-imx5.h:#define MXC_CCM_CSCDR3_HSI2C_CLK_PODF_OFFSET        (9)

./arch/arm/mach-imx/crm-regs-imx5.h:#define MXC_CCM_CSCDR3_HSI2C_CLK_PODF_MASK        (0x3F << 9)

./arch/arm/mach-imx/crm-regs-imx5.h:#define MXC_CCM_CSCDR3_FIRI_CLK_PRED_OFFSET        (6)

./arch/arm/mach-imx/crm-regs-imx5.h:#define MXC_CCM_CSCDR3_FIRI_CLK_PRED_MASK        (0x7 << 6)

./arch/arm/mach-imx/crm-regs-imx5.h:#define MXC_CCM_CSCDR3_FIRI_CLK_PODF_OFFSET        (0)

./arch/arm/mach-imx/crm-regs-imx5.h:#define MXC_CCM_CSCDR3_FIRI_CLK_PODF_MASK        (0x3F)

Is it applicable to i.MXDL? If you have more information then share it with us.

Regards,

Dipali

0 Kudos
Reply