Where to download the latest bsp for iMX6q support?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where to download the latest bsp for iMX6q support?

867 Views
yangao
Contributor III

Hi,

We have a product that uses imx6q and have a build system on top of Yocto to support it. After years development, we want to update to the latest Yocto build system so to have the latest Linux kernel. My question is where to download the latest Yocto build system for iMX6q support (of course we will create our own machine layer to serve our own purpose)?

Thanks,

Yan

Labels (2)
0 Kudos
Reply
1 Reply

811 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yan

it can be found on source.codeaurora.org/external/imx/linux-imx repository
linux-imx - i.MX Linux kernel 

Linux L4.14.98_2.0.0 Documentation

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply