repo init -u git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-3.10.31-1.1.0_beta
From git://git.freescale.com/imx/fsl-arm-yocto-bsp
* [new branch] imx-3.10.17-1.0.0_ga -> origin/imx-3.10.17-1.0.0_ga
* [new branch] imx-3.10.17-1.0.1_ga -> origin/imx-3.10.17-1.0.1_ga
* [new branch] imx-3.10.17-1.0.2_ga -> origin/imx-3.10.17-1.0.2_ga
* [new branch] imx-3.10.53-1.1.0_ga -> origin/imx-3.10.53-1.1.0_ga
error: revision imx-3.10.31-1.1.0_beta in manifests not found
Does it mean 3.10.31 is not supported anymore?
Solved! Go to Solution.
Hi ban
suggest to post this on meta-fsl-arm mailing list
https://lists.yoctoproject.org/listinfo/meta-freescale
~igor
Hi ban
right, it is not more supported (still beta version).
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
Can I download that branch from some other URL? This branch is previously used by us.
Thanks,
Ban
Or is there any branch available which is based on 3.10.31?
Thanks,
Ban
Hi Igor,
Do you mean we can use the yocto branch( fsl-arm-yocto-bsp.git) like,imx-3.10.17-1.0.2_ga, then replace the kernel inside it with http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/log/?h=imx_3.10.31_1.1.0_beta2?
Is there any yocto branch available, which uses 3.10.31 kernel directly, just like git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-3.10.31-1.1.0_beta
Thanks,
Ban
Hi ban
suggest to post this on meta-fsl-arm mailing list
https://lists.yoctoproject.org/listinfo/meta-freescale
~igor
Hi Igor,
Thanks a lot!
Ban