Where to download Ubuntu core for armhf?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Where to download Ubuntu core for armhf?

3,051 次查看
paulchen1
Contributor I

I like to put Ubuntu on the NXP board with an ARM hardware float iMX6 solox processor. But I can't find a place to download Ubuntu core any more as I need to get the compatible rootfs from it. The links are dead

http://cdimage.ubuntu.com/ubuntu-core/releases/14.04/release/ubuntu-core-14.04.4-core-armhf.tar.gz

referred from https://community.nxp.com/docs/DOC-330147

and current links no longer support generic armhf except for a few models:

http://cdimage.ubuntu.com/ubuntu-core/18/

I wonder if you have any idea about what's the cause and where to find compatible core & rootfs now?

Thanks for comments

标签 (2)
0 项奖励
回复
1 回复

2,495 次查看
diegoadrian
NXP Employee
NXP Employee

Hello

It seems that the image is no longer stored on that git. What could I found was the one by Ubuntu 16 and Ubuntu 18:

Ubuntu Core 18.04 LTS (Bionic Beaver) Daily Build and the base image for the 14.04: Ubuntu Base 14.04.5 LTS (Trusty Tahr) 

Unfortunately, Ubuntu is not an official BSP release by our boards, we cannot support those images and I cannot guarantee what If those images will work.

I apologize for the inconveniences this could give you.

Best Regards,

Diego.

0 项奖励
回复