Where to download Ubuntu core for armhf?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where to download Ubuntu core for armhf?

1,823 Views
paulchen1
Contributor I

I like to put Ubuntu on the NXP board with an ARM hardware float iMX6 solox processor. But I can't find a place to download Ubuntu core any more as I need to get the compatible rootfs from it. The links are dead

http://cdimage.ubuntu.com/ubuntu-core/releases/14.04/release/ubuntu-core-14.04.4-core-armhf.tar.gz

referred from https://community.nxp.com/docs/DOC-330147

and current links no longer support generic armhf except for a few models:

http://cdimage.ubuntu.com/ubuntu-core/18/

I wonder if you have any idea about what's the cause and where to find compatible core & rootfs now?

Thanks for comments

Labels (2)
0 Kudos
1 Reply

1,267 Views
diegoadrian
NXP Employee
NXP Employee

Hello

It seems that the image is no longer stored on that git. What could I found was the one by Ubuntu 16 and Ubuntu 18:

Ubuntu Core 18.04 LTS (Bionic Beaver) Daily Build and the base image for the 14.04: Ubuntu Base 14.04.5 LTS (Trusty Tahr) 

Unfortunately, Ubuntu is not an official BSP release by our boards, we cannot support those images and I cannot guarantee what If those images will work.

I apologize for the inconveniences this could give you.

Best Regards,

Diego.

0 Kudos