Where to change drive strength for USB 3.0?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Where to change drive strength for USB 3.0?

1,197件の閲覧回数
parth_modi
Contributor I

Hi All,

We are working on imx8mq processor-based custom design. We used Linux kernel 4.14 for development. We want to change the drive strength of USB 3.0 USB2 port.

The pins are following to needs to change drive strength.

USB2_DN
USB2_DP
USB2_TX_P
USB2_TX_N
USB2_RX_P
USB2_RX_N

Can you please share documents or file name to change this drive strength of USB2 port?

Thanks,
parth

0 件の賞賛
返信
1 返信

1,059件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi Parth,

Please check register PHY_CTL3_ADDR, fields TXRESTUNE0 and TXRISETUNE0.


Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

-------------------------------------------------------------------------------

0 件の賞賛
返信